04 December 2017
This text is the English translation of the official Turkish version of the applicable press release. It has been prepared solely as a reference and ease of use. Please refer to the original Turkish text for details and/or attributes. In case of any incongruity, original Turkish version shall prevail.
Mitsubishi Electric, a sponsor of the International Tunneling Symposium, attracted attention by its innovative technologies
Mitsubishi Electric, the leading brand in the automation industry, supported International Tunneling Symposium organized by the Tunneling Association with Silver Sponsorship. Mitsubishi Electric Turkey Factory Automation Systems Major Projects Business Development and Factory Automation Director Hüsnü Dökmeci, being the spokeman in the event, described the solutions of Marmaray Project, which has a daily passenger capacity of over 500 thousand. Dökmeci providing information about the control system designed by Mitsubishi Electric with a 100% redundant in the world's deepest immersed tube tunnel Marmaray, indicates that everything in the system is ready for passenger safety 7/24.
In the International Tunneling Symposium of Tunneling Association at the Wyndham Grand Istanbul Levent Hotel between 2-3 December with the theme "Challenges of Tunneling" sector representatives met from around the world. Mitsubishi Electric Turkey Factory Automation Systems Major Projects Business Development and Factory Automation Director Hüsnü Dökmeci made a representation in the event that Mitsubishi Electric as the pioneer brand of automation industry provided support with Silver Sponsorship. Dökmeci described the solutions of Mitsubishi Electric, which combines strength with Taisei Corporation, which has a prestigious place in large scale construction projects in the world, in the Marmaray Project, which has the deepest immersed tube tunnel and with a daily passenger capacity of over 500 thousand.
Hüsnü Dökmeci, who stated that realised Marmaray's "Station Information and Management System Project" within the scope of infrastructure projects among Mitsubishi Electric's activities in Turkey, explained that their services of Marmaray in the following way; "Mitsubishi Electric's services at Marmaray BC1 Bosphorus Transition Project cover; high-tech automation equipment, engineering and design, projecting, software programming, hardware assembly, commissioning, training and service support. We carried out control and supervision of electromechanical equipment in the tunnel, all stations, ventilation buildings and generator buildings. Additionally, the scenario required for the Marmaray energy systems to be supplied by two TEİAŞ and two generator sets in both sides.
Within the scope of the Marmaray Bosphorus Transition Project, works which Mitsubishi Electric performed in the tunnels were; control and monitoring the ventilation system, starting, stopping and monitoring the smoke discharge scenarios, opening and closing the flood gates, monitoring the drainage system and monitoring the alarms, monitoring and controlling the illumination, monitoring the environmental measurement systems, monitoring fire alarm and extinguishing systems. The works of our brand in station and ventilation buildings include control and monitoring of common area and room fans, control and monitoring of low voltage distribution and UPS systems, monitoring of fire and extinguishing systems, control and monitoring of common area lighting, monitoring of clean water, polluted and wastewater system, control and monitoring of the stairs, monitoring of the elevators.”
Dökmeci, providing information about Marmaray control system designed by Mitsubishi Electric as a 100% redundant system, esplained that "Marmaray control system with 37 thousand hardware monitoring and control points, 107 thousand software monitoring and control points, 750 operator screen control pages and 100 km communication cable operated 7/24. Therefore, for example, in the event of a fire in the tunnel, the operators can contact the train operator at the relevant incident point and can detect the air flow direction to evacuate the passengers and the smoke. Thus, the system can direct the operator to minimize the possibility of error and easily start the defined ventilation scenario.”
Dökmeci, indicating that all electromechanical systems of Marmaray BC1 Bosphorus Transition Project are monitored by SCADA system called SIMS (Station Information Management System); concluded that "Among these subsystems, tunnel and station ventilation, power distribution systems, lighting, flood gates, fire detection and extinguishing systems have a critical importance. All of this is controlled and monitored in full by Mitsubishi Electric's infrastructure. In the tunnel there is also a fully redundant fiber infrastructure. In each station, the control of the subsystems is provided continuously with redundant PLCs. The continuity of the systems, which is very important in underground subway systems, is an extremely sensitive issue when evaluated in terms of passenger safety.”
Note that the releases are accurate at the time of publication but may be subject to change without notice.