05 December 2017
This text is the English translation of the official Turkish version of the applicable press release. It has been prepared solely as a reference and ease of use. Please refer to the original Turkish text for details and/or attributes. In case of any incongruity, original Turkish version shall prevail.
Mitsubishi Electric introduced innovative solutions at SPS IPC Drives Fair
Mitsubishi Electric, the pioneer brand in the automation industry, informed the visitors at the SPS IPC Drives Fair in Nuremberg, Germany, with the advantages that digitalization has in boosting production flexibility. Mitsubishi Electric, which stands out with its digital factory concept e-F@ctory as a respond to Industry 4.0, introduced innovative technologies in the field of automation with live demos.
Mitsubishi Electric presented a new generation of technologies in the SPS IPC Drives Fair held in Nuremberg, Germany between November 28-30, offering a practical structure for digital transformation in production with the e-F@ctory concept as a response to Industry 4.0. Displaying a live demonstration of how data will be collected for visualization, monitoring and interpretation of production processes and how it can be transferred to a higher-level SCADA system, Mitsubishi Electric served an opportunity to experience digital transformation processes on its way. With this system, which includes three applications that show production processes in real time, users can learn about operational status and performance information, as well as predictive maintenance needs and actions to be taken in this direction.
The three applications in the demo that the brand exhibits at the fair are connected to each other through a MAPS SCADA System where the visualization of the production is used to display the data and the monitoring information on the screen. This network-linked system includes a Guided Operator Solution that works with the principle of an automated product identification system and of semi-automatic zero failure. There is also a Linear Transfer System developed on smart carriages for smart control of product motion processing and transfer. In the application that also includes Complete Factory Automation Solution, which shows the connection of the whole product portfolio, application data received from robot, driver and control systems are transferred live to MAPS application. The processed data is transferred with the cloud, allowing deep analysis of production data and integration with intelligent device applications. The results support new methods for production management and provide transparency for enterprise resource planning (ERP).
Mitsubishi Electric Smart Carriage Technology offers the latest innovations in the modular Linear Transfer System (LTS). In new versions of Smart Carriages, tracks with internal intelligence and data memory can be freely configured (either closed or open circuit). Built-in battery for flexibility such as sensor and holder can be connected on the carriage. When the internal battery is low, it can be used without problems with its functions such as automatically turning to the charging station. Thanks to the Smart Carriages, which can slow down and then stop only the hazardous parts when employees approach a potentially hazardous area and operator safety is ensured without sacrificing efficiency.
In another demo that Mitsubishi Electric exhibited at the fair in conjunction with its production activities in the Industry 4.0 environment included a new addition to the series that works with human without safety barriers. The robot series that works with humans is designed to be close to human in a production environment, unlike industrial robots that have to be placed behind protective barriers for security reasons. Thanks to its ability to work with human, this series can be flexibly positioned anywhere in the production environment. Mitsubishi Electric, which draws attention with the robot series that works with human, offers easy operation with its performance as well as innovative control and programming options. The robotic touch-enabled operator terminal offers an intuitive interface to 'teach' the robot its task without requiring special programming expertise. The teaching function includes a 'direct control' mode that allows the operator to move the robot manually and with controlled power from one position to another. When the installation is complete, the operator terminal is easily removed to allow robots full freedom of movement.
At the fair, Mitsubishi Electric also discussed how to improve quality and efficiency with the Guided Operator Solutions developed for manual installation applications. These solutions enable seamless transfer of production data from manual installation operations to high-end operating systems to support digital transformation in the production environment. The Guided Operator Solutions, which clearly shows the operator which parts need to be picked up and the sequence of operations, helps the increase in quality. This is particularly important in terms of sectors facing increased costs due to potential quality problems and installation operations that are becoming more and more complex nowadays.
At the fair, Mitsubishi Electric also demonstrated PLC's advantages as a platform for automation with a complete set of custom CPU modules for MELSEC iQ-R Series PLC. Available options for analogue and digital I/O, motion, positioning, process control, safety and network connectivity are now complemented by a CNC CPU module integrating the entire control and automation process into a single common platform and a robot control CPU. Modules that offer a complete automation system in a single PLC background provide comprehensive control capabilities while reducing I/O processing times. In addition, the new SIL2 (safety integrity level) certification as well as direct integration with the PLC helps to reduce total operation cycle times and guarantee performance levels.
Mitsubishi Electric's FR-A800-E Series Smart Condition Monitoring (SCM) technology improves the diagnostic capabilities of frequency inverters. Users can perform status monitoring functions directly from the inverter. This additional feature is provided by adding SCM Kit-1 to FR-A800-E series of inverters. Combined with the PLC function and integrated into the FR-A800-E models of the inverter at the same time, this feature offers a complete driver-based solution for preventive maintenance. All of these aspects stand out as the sole example of its kind in the sector. Thanks to this integrated approach to monitoring the status of individual system components, the FR-A800-E series allows for detailed analysis using the red, yellow and green status lights on the sensor. The operating temperature and vibration feedback from the SmartCheck sensor are combined in the inverters by monitoring other external parameters, including speed, voltage and current information. Detailed diagnostics processes can be monitored remotely or displayed on the integrated display of FR-A800-E inverters.
Note that the releases are accurate at the time of publication but may be subject to change without notice.