15 February 2018
This text is the English translation of the official Turkish version of the applicable press release. It has been prepared solely as a reference and ease of use. Please refer to the original Turkish text for details and/or attributes. In case of any incongruity, original Turkish version shall prevail.
Mitsubishi Electric continues to inform manufacturers about the latest technologies compatible with the 4th Industrial Revolution
Mitsubishi Electric drawing attention with its technologically advanced factory automation solutions, in order to inform manufacturers with Industry 4.0 continued its events organized in many provinces of Turkey with Konya. Mitsubishi Electric, which provides added value for rapid integration, productivity and efficiency with high technology and engineering power to Turkish industry, explained automation of heating, ventilation and air conditioning (HVAC) projects with e-F@ctory concept and advanced robotics technology in response to Industry 4.0. It introduced next generation products and solutions, especially Panel Solution Platform and SCADA solution, which collect automation systems under a single roof.
Mitsubishi Electric, designing digital factories that are compatible with Industry 4.0, where productivity in manufacture, energy saving and employee comfort enhance, is working to make the Turkish industry ready for the new industrial era. In this context, Mitsubishi Electric by organizing seminars in several
provinces of Turkey and discussing the latest technologies about Industry 4.0, at its next station met with industrialists in Konya. Mitsubishi Electric, who introduced innovative technologies compatible with Industry 4.0 to industry representatives at Konya Dedeman Hotel, talked about digital factory concept e-F@ctory and advanced robot technologies. In the seminar, information about automation works of Mitsubishi Electric's heating, ventilation and air conditioning (HVAC) projects was given. SCADA solution, Panel Solution Platform and compressor solutions were also presented.
Information on the e-F@ctory concept, which is a response to Mitsubishi Electric's Industry 4.0, was shared in the event which brought representatives from different sectors together. The digital factory concept e-F@ctory, which has emerged as an integrated solution for building reliable and flexible manufacture systems, offers tremendous cost savings while increasing speed, quality and productivity in manufacture. With this concept, Mitsubishi Electric gives an opportunity to industrialists to be able to set up their factories to meet all the needs of Industry 4.0. Before factory investment, it provides an opportunity to construct a virtual factory and realize the simulation of the factory and manufacture, evaluate the productivity and shape the investment in the direction of the outputs. Mitsubishi Electric uses the e-F@ctory concept in its production lines since 2003 and reflects its experience on its products and customers.
One of the highlights of the seminar was Mitsubishi Electric's advanced robot technology. The robot control unit of Mitsubishi Electric, acting with the awareness that the speed and convenience provided by the robots will play a greater role in the industry day by day; provides flexibility of motion control, the speed, accuracy and precision of the system. In addition, with its flexing functions, the robot arm acts as a kind of spring and is stretched according to the force. For advanced applications, Mitsubishi Electric's robots can be easily integrated with conveyor (conveyor belt) and product monitoring, force control and visibility features. The "Sensorless Collision Control" feature allows the robot to detect any obstacle in manual or automatic mode and prevent collision damage.
The RV-F series of Mitsubishi Electric's dynamic 6-axis robot is able to imitate human arm movements and boost productivity using very high speed systems with its 0.32 second cycle times. The dual-arm structure of the 6-axis industrial robot, which can easily perform flexible figures with its dynamic structure, does not only provide added value in terms of freedom of movement, but also offers more stability and versatility. For the RV-F series, it is not difficult to work in very confined spaces and it is no problem to install robots on walls or ceilings. Mitsubishi Electric robots range from 504 to 2.050 millimeters depending on the model, with a carrying capacity of 2 to 70 kilograms.
Mitsubishi Electric, which provides high value added advanced technology automation solutions to the Turkish industry, also introduced the "Panel Solution Platform" which collects innovative automation system solutions under one roof. Platform of the external cabin is produced in Turkey offers the possibility of commissioning at short notice to industrial facilities and infrastructure projects. The "Panel Solution Platform", which enables the automation of many different processes such as fan, pump, compressor, air handling unit, mill, conveyor, crane, crusher, mixer and opening-winding applications much more practically and efficiently, with its ready solution parameters and programs, it also removes the need for additional hardware. This platform has an infrastructure that can provide a complete solution in addition to Panel Solution Platform such as PLC control system solution, low harmonic solution, brake unit and brake resistor solution, panel cooling system solution. In addition, due to its wide range of options and modular structure, it can be preferred either individually or in groups according to the needs of facilities and projects.
Mitsubishi Electric's SCADA solution significantly reduces engineering time spent developing and configuring with wizard interfaces that can automatically create PLC and SCADA projects. It also allows for a standard structure that will facilitate ongoing maintenance of the plant during the life cycle. With MAPS (Mitsubishi Electric Adroit Process Suite), reports can be created automatically covering fields such as input/output plans, PLC and SCADA label configurations. MAPS also helps keeping project documentation up-to-date. Throughout the design phases, and even when the systems are changed or updated over time, MAPS provides uninterrupted management capability for PLC/SCADA projects and facilities according to the installed electrical documentation for the system.
Note that the releases are accurate at the time of publication but may be subject to change without notice.