05 October 2017
This text is the English translation of the official Turkish version of the applicable press release. It has been prepared solely as a reference and ease of use. Please refer to the original Turkish text for details and/or attributes. In case of any incongruity, original Turkish version shall prevail.
Mitsubishi Electric exhibited its innovative solutions at ST Robot Investments Fair
Mitsubishi Electric, participating with the concept of "My Right Arm" in the 3rd ST Robot Investments Fair and Summit which brought the professionals of the factory automation industry and the decision makers of the production and investment processes of factories, exhibited innovative solutions in accordance with Industry 4.0. Flexible, compact, maintenance-free, long life Mitsubishi Electric robots which facilitate production even in the most sensitive processes are candidates for the right-hand of industrialists that they can resign their work. In additon to its talented robots, introducing iQ Automation Platform, Security Solutions and MAPS (Mitsubishi Electric Adroit Process Suite) technology, Mitsubishi Electric also made presentations on its robot technologies and applications.
Mitsubishi Electric, which provides high added value to the Turkish industry with its factory automation products having advanced technology, attended the 3rd ST Robot Investments Fair and Summit held on 4-6 October at the WOW Convention Center with the concept of "My Right Arm". Mitsubishi Electric robots, which are candidates to be right-hands that industrialists can safely entrust their work, have drawn attention with advanced technologies which provide great convenience at every stage of production. Mitsubishi Electric robots operate 24/7 without any maintenance for 25 thousand hours in all conditions, plus minus 240 degrees and a total of 480 degrees of access, providing operational space for installation area for enterprises by minimizing the surrounding dead spaces. Robots can easily be included in the ideal automation chain by communicating with the whole plant by the help of their iQ Platform structure. With their compact structure, robots can be transported to any area of the factory at any time, thus allowing a flexible production space.
Mitsubishi Electric's robot control unit provides the flexibility of motion control, the speed, accuracy and precision of the system. In addition, with its flexing functions, the robot arm acts as a kind of spring and is stretched according to the force. For advanced applications, Mitsubishi Electric's robots can be easily integrated with conveyor belt and product monitoring, force control and visibility features. The "Sensorless Collision Control" feature allows the robot to detect any obstacle in manual or automatic mode and prevent collision damage.
Mitsubishi Electric's RV-F series 6-axis dynamic robot is able to mimic human arm movements and boost productivity using very high-speed systems with the help of 0.32-second cycle times. The dual-arm structure of the 6-axis industrial robot, which can easily handle flexible figures with its dynamic structure, does not only provide added value in terms of freedom of movement, but also offers more stability and versatility. For the RV-F series, it is not difficult to work in very tight spaces, and it is no problem to mount robots on walls or ceilings. Mitsubishi Electric robots range from 504 to 1.503 millimeters depending on the model, with a carrying capacity of 2 to 70 kilograms.
In the fair, in addition to its talented robots, Mitsubishi Electric also presented its industry-compatible solutions such as the iQ Automation Platform, Security Solutions and MAPS (Mitsubishi Electric Adroit Process Suite) technology, as well as presentations on robot technologies and applications.
The iQ Automation Platform, which provided the creation of e-F@ctory concept, being the response to Mitsubishi Electric's Industry 4.0, is one of the few product families that combines all important automation components in one single structure. iQ Platform enables Mitsubishi Electric to work with all automation disciplines, including CNC (Computerized Numerical Control), Motion, Robotics, PLC and Process applications simultaneously and communicate without setting up any communication channel. Mitsubishi Electric iQ Platform minimizes the cost of first investment (TCO: total cost of ownership) by reducing the costs and engineering times which can be created in the entire automation life cycle, increasing productivity and facilitating access to information on the field. With iQ Platform, two or more robots can work in a narrow cell without touching each other and act synchronously with each other.
Mitsubishi Electric MELSEC Safety while providing safety information to be visualised, enhances safety control, and improves productivity. The MELSEC Safety product groups allow the selection of the most appropriate safety control devices for system configuration. Safety PLC, which is well suited for security control applications in medium and large sizes, allows flexible systems to be built using CC-Link IE Field, CC-Link Safety, special ladder programming and function blocks. Safety controller stands out as the ideal solution for small and medium-sized safety control applications and allows easy programming of a safety circuit using only function blocks. MELSEC-Q Safety relay modules, which are offered as an easy way to add a safety circuit without using a program, are preferred for small-scale security control.
MAPS (Mitsubishi Electric Adroit Process Suite) which serves a SCADA program where monitoring and control system are offered, also stands out as a reporting and analysis program. Process design, engineering, control systems development, installation, commissioning and acceptance testing, maintenance, repair and ongoing upgrades add value to all phases of the automation system project.
MAPS developed on MS.NET platform; is compatible with various Microsoft operating systems and database programs such as Microsoft Access, SQL, Microsoft Excel, and Oracle. C #, Visual Basic.net and JavaScript languages can be used internally without any license. Alarm management and intelligent reporting solutions reduce the engineering costs while analyzing the entire system. HTML5-based web client having a dynamic interface, provides remote access from the computer, tablet or smartphone. Vectorial and Windows based graphics can be created easily. They have drivers that can communicate with over 100 manufacturer's devices. By using Microsoft Windows safety, the highest level of protection is provided. Having an OEE (Overall Equipment Effectiveness) function that monitors and improves the effectiveness of production processes, MAPS can control all activities in production with the functions of MES (Manufacturing Execution System) capacity.
Note that the releases are accurate at the time of publication but may be subject to change without notice.