News Releases
This text is the English translation of the official Turkish version of the applicable press release. It has been prepared solely as a reference and ease of use. Please refer to the original Turkish text for details and/or attributes. In case of any incongruity, original Turkish version shall prevail.
5 November 2019
Technology giant Mitsubishi Electric leads the industry with elevators with high speed, comfort, safety and high energy efficiency. With the back-up system used in all elevators of the brand, elevators are made to stop in the closest floor and passengers are safely evacuated in cases such as earthquake and power outage. Installing elevators that don't let a vertically placed coin fall down even at highest speeds in a 70 storey skyscraper in Yokohama 26 years ago, Mitsubishi Electric is incorporating its advanced technology into elevators with specially designed artificial intelligence monitoring system, AI Neural Network. Eliminating the risk of getting stuck between floors with its back-up control software, Mitsubishi Electric stands out with its environment-friendly approach alongside the safety features. Allowing to convert heat energy back into building electric network as usable energy, Mitsubishi Electric elevators provide up to 35 percent energy saving, reducing CO2 emission by nearly 1.400 kg per year. Providing added value to major projects worldwide, Mitsubishi Electric elevators also draws attention with numerous prestigious projects in Turkey as well.
Standing out with its pioneering elevator technologies, Mitsubishi Electric stands as the first company to successfully develop VVVF Inverter control technology for elevators. Installing elevators that don't let a vertically placed coin fall down even at highest speeds in a 70 storey skyscraper in Yokohama in 1993, the brand continues to develop elevators with high speed, comfort, safety and energy efficiency with even more advanced technologies today.
Mitsubishi Electric works with the awareness that, alongside all convenience provided by elevators, users and elevator sector workers should be more perceptive of possible dangers that might occur in erroneous situations. With the back-up control software incorporated into the brand's elevators, elevators are prevented from being stuck between floors during events like earthquake and power outages while a second Back-Up System evacuates passengers from elevators in the case of a problem in the control panel. Incorporating Back-Up System as a standard feature in its elevators which is well-received in Turkey as well as globally, the brand's elevators are listed amongst the most problem-proof elevators in the industry. Minimizing malfunctions in elevators with its advanced technology, quality manufacturing stock, proficiency during assembly and post-sales services, the brand's elevators provide a huge cost advantage as they do not require modernization work for 20-25 years. Creating a difference with its back-up control software alongside top-end safety hardware and software, Mitsubishi Electric leads the elevator industry in terms of "travel comfort, quality, silence".
Mitsubishi Electric developed AI Neural Network which increases operational efficiency and user satisfaction to use specially designed artificial intelligence monitoring system in its elevators. In this system, currency traffic flow is recorded on system computer's memory to minimize waiting times to provide problem-free service with minimum energy waste. Developing smaller elevators with higher energy savings thanks to its advanced technology, the brand removes noise and vibration at ultra-high speed, providing safe and smooth travel comfort.
The technology invented by Mitsubishi Electric, which is only available in Mitsubishi Electric elevators that deciding on the speed of the elevator according to current load provides considerable high energy saving. With the regeneration feature, it is made possible to convert heat energy back into building electric network as usable energy. This system achieves up to 35 percent energy saving, reducing CO2 emission by nearly 1.400 kg per year. Mitsubishi Electric elevators provides high energy saving by switching to sleep mode when no call is made or traffic density is low.
Preferred in numerous prestigious projects in Turkey such as Quasar İstanbul – Fairmont Hotel İstanbul, Rönesans Tower Ataşehir, Tema İstanbul, Bursa Hilton Hotel, Çırağan Palace By Kempinski, Vadistanbul Bulvar and Park Etapları with its elevators, Mitsubishi Electric also leaves its mark in select global projects. Having installed the nation's fastest elevators in LCT Landmark Tower located in South Korea's Busan city, Mitsubishi Electric provides advanced travel comfort, silence and safety in this project with the advanced drive and control equipments it developed for its ultra-high speed elevators.
Note that the press releases are accurate at the time of publication but may be subject to change without notice.